Grove Arduino Library for Kendyte K210 #Sipeed Maix BIT
#Sipeed Maix BIT
#Grove AI EDGE COMPUTING
Since the release of Seeeduino in 2008, Seeed has been contributing software to the Arduino community. Today we have released new software: ArduinoCore-k210.
Based on kendryte-standalone-sdk, we added the full ArduinoCore-API interface to support Arduino IDE, Linux, Windows, Mac OS X and other development environments. With the support of the ArduinoCore-k210, all k210-based development boards can run Grove Arduino Library and many excellent Arduino libraries in the community of Arduino.
Here’s how to use the ArduinoCore-k210:
Use WS2812 on the Sipeed Maix Bit
Use Grove AI EDGE COMPUTING(Just engineering samples) with Grove modules
![](https://blog.seeedstudio.com/wp-content/uploads/2019/04/2201555058096_.pic_-1030x1030.jpg)
ArduinoCore-k210 is also supported as a normal IDE. For example, when developing kendryte-standalone-sdk, you also can use the Arduino Library WS2812FX.
#include <WS2812FX.h>
#define LED_COUNT 32
#define LED_PIN 13
#define TIMER_MS 5000
// Parameter 1 = number of pixels in strip
// Parameter 2 = Arduino pin number (most are valid)
// Parameter 3 = pixel type flags, add together as needed:
// NEO_KHZ800 800 KHz bitstream (most NeoPixel products w/WS2812 LEDs)
// NEO_KHZ400 400 KHz (classic ‘v1’ (not v2) FLORA pixels, WS2811 drivers)
// NEO_GRB Pixels are wired for GRB bitstream (most NeoPixel products)
// NEO_RGB Pixels are wired for RGB bitstream (v1 FLORA pixels, not v2)
// NEO_RGBW Pixels are wired for RGBW bitstream (NeoPixel RGBW products)
WS2812FX ws2812fx = WS2812FX(LED_COUNT, LED_PIN, NEO_RGB + NEO_KHZ800);
unsigned long last_change = 0;
unsigned long now = 0;
extern “C” {
#include <stdio.h>
#include <unistd.h>
#include “fpioa.h”
#include “gpiohs.h”
#include “sysctl.h”
uint32_t irq_flag;
#define PIN_LED 25
#define PIN_KEY 26
#define GPIO_LED 3
#define GPIO_KEY 2
uint32_t g_count;
int irq_gpiohs2(void* ctx)
{
irq_flag = gpiohs_get_pin(GPIO_KEY);
printf(“IRQ The PIN is %d\n”, irq_flag);
uint32_t *tmp = (uint32_t *)(ctx);
printf(“count is %d\n”, (*tmp)++);
if (!irq_flag)
gpiohs_set_pin(GPIO_LED, GPIO_PV_LOW);
else
gpiohs_set_pin(GPIO_LED, GPIO_PV_HIGH);
return 0;
}
int main(){
#define NOFREERTOS 1
plic_init();
sysctl_enable_irq();
fpioa_set_function(PIN_LED, FUNC_GPIOHS3);
gpiohs_set_drive_mode(GPIO_LED, GPIO_DM_OUTPUT);
gpio_pin_value_t value = GPIO_PV_HIGH;
gpiohs_set_pin(GPIO_LED, value);
fpioa_set_function(PIN_KEY, FUNC_GPIOHS2);
gpiohs_set_drive_mode(GPIO_KEY, GPIO_DM_INPUT_PULL_UP);
gpiohs_set_pin_edge(GPIO_KEY, GPIO_PE_BOTH);
gpiohs_irq_register(GPIO_KEY, 1, irq_gpiohs2, &g_count);
ws2812fx.init();
ws2812fx.setBrightness(255);
ws2812fx.setSpeed(1000);
ws2812fx.setColor(0x007BFF);
ws2812fx.setMode(FX_MODE_STATIC);
ws2812fx.start();
while(1){
now = millis();
ws2812fx.service();
if(now – last_change > TIMER_MS) {
ws2812fx.setMode((ws2812fx.getMode() + 1) % ws2812fx.getModeCount());
last_change = now;
}
}
return 0;
}
}
“`
ArduinoCore-k210 is a very interesting software project to help all of you develop AI in an easier way. We can’t guarantee that there is no any of bug. If you encounter any compatibility issues or have any new ideas, feel free to check our GitHub link and forum to communicate with us, we will try our best to solve the problems you have encountered. This is the ArduinoCore-k210, hope everyone likes it!