#newproductsTuesday – All-new Grove Base HATs for Raspberry Pis
Hey Seekers!!!
It’s newproductsTuesday!!! Today we are going to introduce 2 Grove Base HATs for Raspberry Pis. They are the Grove Base HAT for Raspberry Pi and the Grove Base HAT for Raspberry Pi Zero.
Both these HATs use an STM32F030 as ADC and have an output voltage of 3.3V. They already support more than 60 Grove modules. Also, they are compatible with the following Raspberry Pi models.
- Raspberry Pi 2/3 Model B/B+
- Raspberry Pi Zero
These HATs stand out because of the very low cost compared to GrovePi+.
Grove Base HAT for Raspberry Pi
- 15 Grove connectors:
- 6 x Digital, 4 x Analog, 3 x I2C, 1 x UART, 1 x PWM
- Provides an 8-Channel ADC
Grove Base HAT for Raspberry Pi Zero
- 8 Grove connectors:
- 2 x Digital, 3 x Analog, 1 x 2C, 1 x UART, 1 x PWM
- Provides a 6-Channel ADC
Check out the video below to see a cool demo and learn more about our new Grove Base HAT for Raspberry Pi and Pi Zero.