They’re Finally Here! Introducing New Fusion Mini Stencils

Seeed Fusion Mini Stencil vs the smallest framed stencil
Small and light as a (metal) feather
The new stencils are only a few grams in weight and can fit into the smallest Seeed Fusion packages, protective wooden boards included. That means you can use the cheaper airmail services or simply save heaps of money on express shipping. To the USA for example, with the mini stencils, you can save half on DHL shipping costs and save over 70% by using standard airmail.Smaller but just as good
These stencils are made with the same stainless-steel material as our regular stencils and so will have the same solder paste depositing accuracy. The corners have also been rounded off and the edges smoothened to make them safer and easier to handle. Us folks at Fusion are very excited to introduce the mini stencils. It is not every day that Fusion can bring you a new product, and we know you have been anticipating these for a while. Many of you were put off ordering stencils before since the stencils were huge, heavy and as a result, incurred nasty shipping costs. Not great if you only need a few tiny footprints for a single board. Now with a smaller, lighter and somewhat cuter option available, there is no reason not to give our stencils a try. Get them for only $8.90USD on the Seeed Fusion Stencil order page here:
This is great news! Do you maybe also plan to offer plastic stencils? Most often they are good enough for prototypes but also much cheaper than stainless seel.
Nice suggestion! Plastic stencils are not as common as the standard metal ones and are not as precise but we’ll keep an eye out for them
Question: Is the design automatically centered in the stencil or is it aligned with an edge of the stencil’s effective area (maybe top/left)?
It’s centered
First you drop the prices of bare pcb board and now the stencil !
You guys rocks making electronics prototyping way easier and accessible !
Thant’s a great news for all makers out there.
I ll definitly build my own reflow oven this year !
Awesome! We can help out with the oven!