PCB Assembly Process Steps
![](https://blog.seeedstudio.com/wp-content/uploads/2021/04/微信图片_20210407164202-1030x268.png)
With the continuous development of SMT technology, the level of SMT automation has been continuously improved, and more advanced equipment has been added, and the corresponding production process has also changed. In this field, Seeed Fusion assembly workshop provides advanced equipment and consummate soldering technology.
Let’s see how Seeed Fusion provide such service and this is the flow chart for the main production steps of PCB assembly process.
Materials Preparation
1. PCB (print circuit board): Check each board and make sure there is no short circuit, broken circuit, blurred silkscreen or any other quality issues.2. Components: Make sure the component is complete, pay attention to the foot oxidation of the component, also need to check there is no oil and the polarity of the components.
3. PCB Stencil and Solder Paste: Take out the solder paste from the freezer, It needs thawing, stirring.
4. Gerber file and BOM list on the desk.
5. Tools: Soldering iron, tin, wire stripper, component box, torch, pliers, heat gun and so on.
Bare Board Baking
Ensure the dryness of PCB
Solder Paste Printing
The solder paste stencil printing machine accurately printed to PCB pad.
Pre-Soldering Inspection
Check the boards to ensure that there is no problem for soldering.
High Speed Mounting
The pick and place machine can attach the components accurately to the PCB plate by drawing the components.
Visual Inspection Before Re-Flow
Check the board to ensure that there is no problem for Re-flow soldering.
Re-Flow Soldering
Install components onto the PCB and put it in the reflow machine, the components are soldered by using drying area, the preheating area, the welding area, and the cooling zone.
AOI
After the print circuit board has completed the soldering, the AOI instrument is used to detect the soldering of the PCB.
DIP plug-in processing
The DIP production line colleagues make a simple processing of the plug-in material and insert the corresponding position of the board.
Wave Soldering
Put the plugged board into the wave soldering, the soldering of PCBA board is achieved through the spray welding flux, preheat, wave peak soldering, cooling, etc.
Cleaning
To make sure there is no defects on the board after wave soldering, which usually needs to be washed.
ICT/FCT
Generally, the PCBA board should be ICT, FCT, aging test and program burning, in order to ensure the normal operation of the PCBA function and reduce the rework rate in the later period.
Quality Checking
The finished product needs to be sent to the quality inspection department for quality checking, make sure there is no quality issue before packing.
Packing
Coming to the last part, we use antistatic bags for packing
The above is the assembly process of PCBA. We believe that you can know how it work after you have read it.
Seeed Studio Fusion offers one stop high-quality, low volume yet affordable PCBA service with 10 years’ experience, please use Seeed Fusion to fabricate your artistic product.