[50] Generally, solder mask will cover copper traces, but in special cases, traces can be exposed according to
the specific requirements.
6.2 Solder Mask Design for Holes
6.2.1 Via Holes
[51] Via holes should have solder mask openings on both sides of the board centered about the hole, as shown
in Figure 33. The required diameter of the opening should be D + 5mil where D is the diameter of the plated
hole.
Figure 33: Solder Mask opening for via holes.
6.2.2 Alignment Holes
[52] For metallic rivet holes, the solder mask opening should be centered about the rivet hole with a diameter +
6mil of the plated pad, on both sides.
Figure 34: Metallic rivet hole solder mask opening.
[53] For non-plated rivet holes, the solder mask opening should be greater than the clearance area for the screw
head.
Figure 35: Non-metallic rivet hole solder mask opening.
[54] The solder mask openings for Type A wave soldered holes should satisfy:
Figure 36: Type A mechanical hole solder mask opening.
6.2.3 Positioning Holes
[55] The solder mask opening on the front and back sides of non-plated holes should be D +10mil, concentric
about the hole, where D is the diameter of the non-plated hole.
Figure 37: Solder mask opening for non-plated mechanical holes.
6.2.4 Buried and Plugged Vias
[56] Internal vias (buried vias) do not require solder mask openings on either side of the board.
[57] For PCBs requiring wave soldering or if the board has BGA (or CSP) with a pitch smaller than 1.00mm,
the BGA via hole should be plugged.
[58] If an in circuit testing (ICT) point is added under the BGA, it is recommended to lead out the testing pad
from the via hole as shown in figure 38. The diameter of the test pads should be 32mil; solder mask opening is
40mil.
Figure 38: BGA Testing pad.
[59] If the PCB does not require wave soldering, and the pitch of BGA components is greater that 1.00mm,
then there is no need for plugged vias. The BGA via itself can be used as a test point. The top side solder
mask opening should be 5mil bigger than the diameter of the hole. The bottom side testing pad should be
32mil with a solder mask opening of 40mil.
6.3 Solder Pad Solder Mask Design
[60] Solder mask design for copper pads should follow figure 39.
Figure 39: Solder mask openings for copper pads
[61] Since PCB manufacturers have limited precision and limits on the minimum width of solder mask
openings, solder mask openings should be at least 6mil bigger than pad size (3mil each side), with a minimum
solder mask bridge width of 3mil. There must be solder mask separating pads and holes to prevent solder
bridges from forming and causing short circuits.
Figure 40: Solder mask openings and material widths for various copper pads.
Table 7: Recommended minimum solder mask material width between pads.
[62] Groups of SMD pads less than 0.5mm (20mil) apart or less than 10mil between the pad edges do not need
solder mask to separate them and can be opened as a group. See figure 41.
Figure 41: Solder mask openings for fine pitch SMD components
[63] Solder mask openings are recommended for heatsink contacts.