Seeed & Intel in China Hi-tech Fair – The First Public Appearance of Genuino 101 in China
As the China Hi-tech Fair is open during this week in Shenzhen(China). Seeed’s showcase in Intel’s pavilion will bring you a wonderful experience. Continually focus on Seeed ,more latest exciting news from this event will be updated for you!
Each year, CHTF is co-hosted in Shenzhen by Ministries and Commissions of the national government and Shenzhen Municipal People’s Government. Up to now, 16 CHTFs have been successfully held in succession. For each CHTF, the total exhibition area exceeded 100,000㎡, nearly 3,000 exhibitors from more than 50 countries and over 500,000 visitors attended. Currently, it is the largest and the most influential scientific and technological fair in China and is renowned as “the No.1 Technology Show in China”.
In Makers’ area, Seeed and Intel show cooperatively. All the demos were co-branded with Intel Edison and designed to create a better ecosystem for the development board.Grove Indoor Environment Kit for Intel® Edison
A functional kit to help explore and interact with indoor environment. Developers can plug up to 11 different Grove sensors and actuators quickly, including Grove – Temperature & Humidity Sensor, Grove – Moisture Sensor, Grove Light Sensor, Grove – UV Sensor and Grove – PIR Motion Sensor, which makes it perfect to create complete smart home applications with Intel Edison and Arduino Breakout Board. All the modules were packaged into a compact blue case, which can be also utilized as the work base.
Xadow Wearable Kit for Intel® Edison
Based on the wearable friendly – Xadow family, the kit includes an expansion board together with eight tiny and powerful Xadow modules, covering sensors, actuators, displays and communication parts, such as Xadow – Q Touch Sensor, Xadow – NFC, Xadow – Vibration Motor, Xadow – 3 Axis Accelerometer, Xadow – Barometer BMP 180 and Xadow – OLED. It also contains a full-color printed tutorial which enables to develop wearable devices with Intel Edison technology quickly.
Robotics 4WD demo
Edison 4WD Auto Robotic Platform 2.0 is fundamental development platform which is based on Intel Edison and features powerful scalability. It can helps inventors, entrepreneurs, and consumer product designers develop more practical and various robots easily. Right in this page, we will show you a simple and cool application.
You only need to connect the Wi-Fi from the little car and control it whatever you want. This product will be available online soon!
Genuino 101 – The first public appearance in China!
“Learning and development board that delivers the performance and low-power consumption of the Intel® Curie™ Module with the simplicity of Arduino at an entry-level price. It keeps the same robust form factor and peripheral list of the UNO with the addition of onboard Bluetooth LE capabilities and a 6-axis accelerometer/gyro to help you easily expand your creativity into the connected world. It is the first public appearance in China.”“The module contains two tiny cores, an x86 (Quark) and an ARC, both clocked at 32MHz. The Quark core runs ViperOS RTOS and helps the Arduino core to accomplish the most demanding tasks. It comes with 14 digital input/output pins (of which 4 can be used as PWM outputs), 6 analog inputs, a USB connector for serial communication and sketch upload, a power jack, an ICSP header with SPI signals and I2C dedicated pins.
The board operating voltage and I/O is 3.3V but all pins are protected against 5V overvoltage.” @Arduino.cc
Know more about Seeed products, click Bazaar.