Weekly New Products Release: Create Your Own phone with RePhone Kit!

Hello Everybody! Something big is happening in Seeed this week and already caused a big sensation to the world! We’re so proud to introduce them to you. Check out what’s brand new this week!

1)RePhone Kit – World’s First Open Source and Modular Phone

Big news! You can create a phone yourself in minutes and hack a new way to communicate with things. RePhone is a set of tools and components that allows everyone including students, teachers, makers, hackers, geeks, artists, developers and engineers rethink, remix, redesign and remake the phone. It comes in three kits RePhone Core Module GSM + BLE, RePhone Core Module 3G and RePhone kit Create. Support us and check out more on Kickstarter.

banner上

2) Raspberry Pi 2.2’TFT Display Module/WOT Touch

Looking for a higher refresh rate screen for Raspberry Pi? The PI-TFT22A module is a good choice for you. It features a 2.2’display with 320×240 16-bit color pixels. The greatest part is that this PI-TFT22A module refresh it’s screen rapidly because the TFT module communicates with raspberry Pi in a high speed SPI interface. The module can be used as Xwindow port ,displaying images or video etc.

317080020

3) Raspberry Pi RTC Expansion Module

Raspberry Pi is quite hot those days. We will introduce you a RTC module which is specifically designed for Raspberry Pi. It communicat with Raspberry Pi through I2C bus. There is a Maxim DS1307 and CR1220 button cell on the board to keep the real time for a long time after the Raspberry Pi has its power down. Set a serial port, TTL convenient way online debugging.

317990036

4) Grove – Sunlight Sensor

Summer is coming, want to make a UV detector to know the UV index when you are under the sun? Grove – Sunlight Sensor is recommended here. Grove – Sunlight Sensor is a multi-channel digital light sensor, which has the ability to detect UV-light, visible light and infrared light. You can use this device for making some project which need to detect the light, such as a simple UV detector.

101020089

About Author

Calendar

September 2015
M T W T F S S
 123456
78910111213
14151617181920
21222324252627
282930