Bluetooth Arduino for the mobile age: LightBlue Bean+ is LIVE on Kickstarter this week!

HeaderImage-CrossPlatform-WithLogo

The most talented BLE Arduino with Grove Connectors – LightBlue Bean+ is launched at Kickstarter this week for crowd funding. With four new Bluetooth Low Energy profiles, solderless connectors, 16 GPIOs, a rechargeable battery and enough range to program neighbor’s neighbor’s Beans, the Bean+ has become the latest addition to the LightBlue Bean family: a line of easy-to-use, wireless Arduinos. It can be wirelessly programmed from OS X, Windows, iOS and Android platforms.

HardwareFeatures

The Bean+ comes with a built-in accelerometer, temperature sensor, RGB LED and a new amplifier. There are two Grove connectors (Analog and I2C, respectively) added for users to hook up with a variety of Grove sensors quickly and easily. There is also a Grove shield that adds 8 more. “We’re proud to see Grove connectors got adopted and excited to help build up the synergy.” Said Eric Pan, founder and CEO of Seeed Studio.

Grove+Seeedstudio_original

Pick and choose your Beans now! Alone, or with a grove starter kit consisting of a potentiometer, buzzer, touch sensor, button and a 10 segment LED bar, ready to be plugged in. Or go big with the perfboard shield and a grove shield that lets you plug in up to 18 grove accessories to one Bean+.

About Author

Calendar

August 2015
M T W T F S S
 12
3456789
10111213141516
17181920212223
24252627282930
31