Catch of Portable RF Explorers and Full Accessories at Hamvention 2015!

Hamvention banner_V1

Shenzhen, China (May 5, 2015) Seeed Studio, the company provides accessible open-source hardware and agile manufacturing service for makers to grow inspirations into differentiating products, will join hands with NutsAboutNets to showcase an array of RF explorers along with various accessories at Hamvention (Booth #342) in Dayton, Ohio, USA during May 15-17.

RF Explorer is an affordable Handheld Spectrum Analyzer designed from scratch to be a sort of Swiss Army Knife for the specific needs of digital radio frequency communication. Compared with traditional commercial expensive and bulky spectrum analyzers, RF Explorer offer 90% of the function at only a 5% of the cost. Additionally, it can be carried on easily anywhere, used outdoors efficiently for hours with a single battery charge.

The hands-on demonstrations onsite will include the following:

A few accessories such as LTE antennas, BNC/SMA adapters, and RF cables will be displayed together as well. You can ask questions, take demos and see the product family first hand. P.S. We offer 10% off discount for any onsite purchase.

We look forward to seeing you soon.

 

About Hamvention

Hamvention is one of the largest and premiere Amateur Radio shows and flea market. Since 1952, Hamvention® has been sponsored by Dayton Amateur Radio Association (DARA). For many years it has been attracting thousands of hams from across North America (and the world) converge to one location to see hundreds of commercial and flea market vendors.

About Author

Calendar

2015 年 5 月
 123
45678910
11121314151617
18192021222324
25262728293031