Guess&Giveaway #SeeedHit 7th

I couldn’t wait to show you the project – .

Let’s take a initial look without the solar panel, it’s made up of

  • 1 LinkIT ONE with antenna
  • 6 sensors
  • 1 base shield

It seems to be a outdoor data logger~

A624028E1770908543DC545FF61C8679

So, what are those Grove sensors, have a look from the behind.

BD562504E0E33F926E4A201BA080007A

Those sensors are:

  • Barometer (BMP180)
  • Light sensor
  • 3-Axis digital accelerometer
  • UV sensor
  • Tem & Humi
  • Dust sensor

Wow, it’s an automatic weather station with GSM short message warning feature. The shell is not water proof, it’s not well designed yet. The 3-Axis digital accelerometer is added to detect accidental falls.

8D15748B5B75299BD50E3ED64E47AEEF

There’s even something hide behind, a lipo rider acts as the bridge between lipo battery and solar panel.

We agree that sam’s answer is detailed and constructive, congratulation!

Here goes the puzzle:

F20AB99154E428EC964B4346C56DDFC6

 

About Author

8 thoughts on "Guess&Giveaway #SeeedHit 7th"

  1. This seem to be a Grove based heart rate pulse sensor.
    There are optical sensor and the enclosed bright LED build into a single component.

  2. This one looks to be an optical pulse sensors. I see transistors and caps that are a little confusing but a closer look points to a reflective type pulse/oxymetery sensor.

Comments are closed.

Calendar

April 2015
M T W T F S S
 12345
6789101112
13141516171819
20212223242526
27282930