Weekly New Products Release

Here we got some new awesome products in Seeed Bazaar this week.
Want to learn more details? Read the following instructions and you will find your favorite!

1) Solar Charger Shield v2.2
The solar charger is a stackable shield to Arduino compatible platforms, enables adaptive battery power and act as energy harvester for in-field charging. You may use various batteries that has the voltage of 3.0V-4.2V to shift up for 5V output, or put on Li-ion battery and solar panel to form an autonomous sensor unit. The maximum current provided by the board can get up to 600mA. An usb connector is also useful to charge the battery.
1

2) Grove – IMU 10DOF v1.0
Grove – IMU 10DOF is based on MPU-9250 and BMP180, it combines a 3-axis gyroscope, 3-axis accelerometer, 3-axis magnetometer and barometer in standard Grove module. Total 10 degrees of freedom make it suitable for mobilephone, aircraft, smart watch etc.
2-   Grove - IMU 10DOF

3) Grove-Digital Infrared Temperature Sensor
Making it very powerful, rich social environment and market value. The more people participate, the more rapid development, the greater the potential market, followed by the more purposes. Currently, besides the children’s education above-mentioned,it also can be used as basic computer, home theater HD player etc.
3-Grove-Digital Infrared Temperature Sensor

4) Doppler X band Radar detector sensor module 10.525GHz
This is a Microwave moving object detector which is designed by Doppler Radar principle.
It is mainly used in automatic door control, safety guard system, automatic video control system, etc. This module use 10.525 GHz band to detect moving.
4-Doppler X band Radar detector sensor module 10.525GHz

5)2.4G wireless module NRF24L01+PA+LNA (PA-IPX)
This wireless Transceiver module is an easy and suitable module if you want to setup your wireless communication system with low cost.
It can achieve a good balance between wireless transition performance and cost.
You can easily add it with your own MCU/ARM/PIC/AVR/STM32 system.
What’s more, this nRF24L01+ module is designed with Power amplifier and IPX antenna This allowed you to use the wireless communication up to 1000 meters.(No barrier)
5-2.4G wireless module NRF24L01+PA+LNA (PA-IPX)

6) WRTnode Standard Shield
Play the shield pls notice that
1. Be sure to plug the WRTnode into the shield as the picture, Be sure DONOT go wrong direction.
2. For the power we recommend a 5V USB-interface adapter higher than 1000mA, when more USB devices plugged in, we recommend a 2A or 2.5A adapter, such as your ipad one.
3. How to with U-Boot web-page fail-safe de-brick button:
4. An original WRTnode U-Boot WRTnode_U-Boot_instructions will provide this, if there’s another U-Boot have been flashed, this section is invalid.
6-WRTnode Standard Shield

7) Raspberry Pi 0.96” OLED Display Module
Raspberry Pi 0.96’ OLED display module is designed by 52pi which is made by 128×64 yellow and blue OLED pixels , diagonal is only 0.96 inch . The controller is SSD1306, communicates via 4-wire SPI, the display have its own backlight, no backlight LED is required ,This reduces the power required to run the OLED and is why the display has such high contrast , extremely wide viewing angle and extremely operating temperature.
7-Raspberry Pi 0.96” OLED Display Module

8) USB Power Adapter – European
A typical European USB power plug adapter to charge your Firefly at home, in the office or any places that can connect to a computer. This power adapter can provide an efficient charging, which wonderfully match the Firfly-RK3288.
8-USB Power Adapter - European

9) SODAQ Mbili rev.5
The SODAQ (Solar Data Acquisition) is an Arduino compatible data acquisition board designed by Gregory Knauff. This is the successor to the SODAQ Moja that we Kickstarted last year. All the experiences and comments we got from our user we combined in this new board, which one of the most rich-featured Arduino Compatible boards in the market.
9-SODAQ Mbili rev.5

10) Triangle RGB LED Brick – WS2812B Breakout(10 PCs pack)
This is a mini breakout board for WS2812B RGB LED. The WS2812B is an 5050 RGB LED integrated with intelligent control chip, including digital port data latch and signal reshaping amplification drive circuit. It can achieve up to1024 points of cascading (refresh rate at 30fps), every pixel is individual addressable and has 256 kinds of brightness display and 1677212 kinds of color variance.

The breakout is designed to be a LED brick. It is the shape of an equilateral triangle, of which, one side for signal input, and the other two are for optional signal output. By various combinations, they can be spliced to be a LED panel or even a LED cube.
10-Triangle RGB LED Brick - WS2812B Breakout(10 PCs pack)

11) TinyTiM LED board
TinyTiM is an 8×8 (64 nos) array of smart RGB pixels that can be controlled from a single microcontroller pin!
11-TinyTiM LED board

12) Energy Monitor Shield V2
Energy Monitor Shield V2 is Arduino-compatible expansion card designed for building energy monitoring system with the ability to connect I2C OLED-display and built-in wireless transceiver nRF24L01 +. Unlike version 1, has on-board interface phototransistor to read data from the built-in LEDs of different counters and interface RS485.
12-Energy Monitor Shield V2

About Author

Calendar

April 2015
M T W T F S S
 12345
6789101112
13141516171819
20212223242526
27282930