Xixi is coming to San Francisco(Be Sure to Wear Flowers in Your Hair) #makerfaire
Xixi is coming to Maker Faire Bay Area, don’t miss the world travel suitcase which contains almost all featured products of Seeed. And it will tell you the GPS location and air quality data of where it is via an OLED screen. You can see it in various maker gatherings. Take a photo and tweet it. You can @seeedstudio and join #TravellingSuitcase to see its world tour.
Xixi upgrates from the suitcase used for exhibition last year. Not only does it contain a bundle of Shields & Grove modules, it also provides the sensor information from the trunk when connected to internet.
The project is open source on Github.
Shield is a special word for board that mounts on an Arduino to give it some amazing capability. Shields from Seeed come in all different flavors from Music Shield to GPRS Shield. There’s such a wide range available that you can play with every popular topic with a shield we provide. No matter what projects you are going to make; a music instrument, an electroluminescent display or even a phone to make calls and send texts, you can find the ingredients here at Seeed.
Grove is a modular, ready-to-use tool set. Much like Lego, it takes a building block approach to assembling electronics and much easier than using a breadboard and various electronic components to assemble a project.
Journey
Xixi’s World Maker Faire tour began last summer.
picture: MAKE
Xixi @PARC,Palo Alto.
Xixi @Rome:
Xixi @Tokyo
Xixi @Shenzhen
Xixi is looking forward to seeing you at Maker Faire Bay Area (Seeed’s booth(EXPO HALL 202) this weekend. Map here
Xixi will also attend SolidCon (Booth # P7) on May 21 & 22 in San Francisco. Welcome to come & say Hi to Xixi as well as chat with some familiar faces from Seeed Studio