Raspberry Pi Accessories – May Theme Review

We had a busy May, focusing on cool accessories for the Raspberry Pi.  They are absolute must-haves for a full Raspberry Pi experience especially for those of you on the go this summer.  Check out these items and stock up before your next trip.

RPI3

Are you aware that the Raspberry Pi can accommodate standard peripherals? Although it’s convenient to attach a full-sized keyboard or a 15” monitor, it’s not feasible when you want to pack up your backpack and go. So we have several options to give you the true minicomputer experience.For your viewing pleasure we have a 7’’ high resolution monitor with a top of the line LCD flat-panel display. It uses TFT technology, so the picture is clear and the power consumption is low. It’s compact, functional and supports VGA, NTSC, PAL, and HDMI signals.

We also have a mini wireless keyboard with built-in touchpad. This is a versatile 3-in-1 solution. It acts as a keyboard, a mouse, and a touchpad. It has a QWERTY style keyboard with multi-language support that fits conveniently in the palm of your hand, and it’s back-lit by LEDs which helps in low light conditions. It even has arrow keys to page up, down, left or right, just like your keyboard at home.  Plus it comes with a USB adapter dongle which allows you to easily pair the keyboard with the Raspberry Pi.

If you want to take advantage of any wireless Ethernet networks, we have an 802.11b/g/n 150Mbps wireless USB adapter. What if your USB ports are already maxed out? No worries, we also have a USB hub to increase your available USB ports! With extra ports, you can expand your options even further, like adding a mini cam. The mini webcam has a high resolution CMOS sensor that provides an image resolution of 300k pixels and has a refresh rate of 30 FPS (frames per second.) It is great for network conferencing, video chatting, or recording video.

In addition to the gadgets mentioned above, we have even more Raspberry Pi related products to choose from. Find additional items by typing Raspberry Pi in the search bar! Or if you are more familiar with the Beagle Bone or Beagle Bone Black embedded systems, all of these accessories will work with them as well.

About Author

Calendar

June 2013
M T W T F S S
 12
3456789
10111213141516
17181920212223
24252627282930