Customized Christmas Ornaments? The Eggbot can do!
Decorating Christmas Ornaments with the Eggbot source from Evil Mad Scientist Laboratories.
As we are approaching that time of year when conifers tend to sprout up in living rooms, here are some techniques and tips for making awesome personalized ornaments with the EggBot.
Check out these beautiful ornaments created by Eggbot folks.
The Eggbot is an open-source art robot that can draw on spherical or egg-shaped objects from the size of a ping pong ball to that of a small grapefruit– roughly 1.25 to 4.25 inches in diameter (3 – 10 cm). The kit is based on the original design by Bruce Shapiro, dating back to 1990.
The Eggbot is super adjustable, and is designed to draw on all kinds of things that are normally "impossible" to print on. Not just eggs but ping pong balls, light bulbs, mini pumpkins, and even things like wine glasses– with a bit of work. As seen in above photos, you can make super personalized Christmas ornaments with the Eggbot!
The Eggbot is now also available at Seeed Studio!