New Product Post
To develop a project that will be used to add some efficiency to your supply chain? You should check this item-Grove-125KHz TFID Reader. It’s a module used to read uem4100 RFID card information. The RFID tech has been spread out in many daily details. You may encounter some things with that when you check out in Wal-mart. Dose anything else flash out? I am thrilled that the Egg-bot kit is finally ready to come to the stage. The Eggbot is an open-source art robot that can draw on eggs or egg-shaped objects. With abundant examples prepared, the second you finish the assembling work, you can start to draw your craft! Let’s just skip the alignment job and have some fun first! But after all, getting down to alignment can’t be avoided for a perfect egg~ Maybe someday I will prepare a video showing some skills about how to simplify this step.
Coming next, Diavolino (“little devil”). It is a low-cost, easy to build Arduino-compatible development board, with the form factor of an Arduino Duemilanove or Arduino Pro, but with nicely rounded corners and a striking appearance. What do you think of its rocky look?
The Bulbdial Clock is an electronic soldering kit to make your own desk/mantle clock. This kit comes from the same supplier we just mentioned. And it remains a consistent style, look like fun mixed with a little mystery. I like two different cases are included for me to choose, a clear one an a black one. What about you?
B-Squares(Super Recipe Kit) is a 3D modular electronics system with an emphasis on solar power and expandable energy storage, enabling the hobbyist to prototype clean-tech and Arduino inventions faster than ever before. The Squares have magnetic contacts on each corner which allow them to easily snap together without wires. These magnetic contacts are also used to transmit electric signals between the Squares. This design allows users to quickly assemble Squares into arrays, with power flowing through the array, without wiring or soldering.
Each Square has individual personality according to their roles. Let’s check some Squares! Here comes the Arduino-SQUARE. This one contains a 3.3V Arduino Pro compatible microcomputer.
And another Battery-SQUARE includes three internal rechargeable AAA batteries. Store your solar power and boost other SQUARES!!
LEDs are always on the table of makers, so does this bold super kit. A LED-SQUARE is included which contains some bright white LEDs and some RGB ones.
The last square is the Proto-SQUARE. It’s there for the case that your circuit need some extra complexity. With this, you can remain the neat and simple look of the whole construction.
The magnetic contacts are used to transmit electric signals between the Squares. How do these work? en…...