Deadline for OSHW logo submission EXTENDED TO March 3rd!

(Via Open Hardware Summit)

With the Open Hardware Definition, we would like to release a logo for Open Hardware to be attached to the definition, and used to brand Open Hardware. Please propose your logos, or comment on the below ones at the Definition Forum under the thread OSHW LOGO.

Criteria:
The logo for the Open Hardware Definition must:

  • Be easy to print/see on a PCB
  • Be easy to print/see on a Schematic document
  • Signify Open-ness

Submission
Submit your logo in jpg or png format to the Definition Forum under the thread OSHW Logo. Please include the following information:

  • Title:
  • Designer:
  • Submitted by: (if different than Designer)
  • Date:
  • Description:

To look at the logos submitted to date, check the  logo page

Selection:
The selection process will be a combination of a committe pre-selection and then a public vote of the community. More details to come soon.

Prize:
Getting to be the person who designed the OSHW LOGO!

Go ahead and join the competition and GOOD LUCK!

About Author

2 thoughts on "Deadline for OSHW logo submission EXTENDED TO March 3rd!"

    1. Sure, i will post them in blog soon. We are pretty busy after the spring festival.. This should be done earlier.

Comments are closed.

Calendar

March 2011
M T W T F S S
 123456
78910111213
14151617181920
21222324252627
28293031