[Survey] What’s holding you back from hacking a DSO nano?

I didn’t realize how difficult it was to hack the DSO nano with a new UI or just adding my signature.  Lacking of documentation, this quest is nearly like reverse engineering. We will put much more efforts on the technical support on DSO nano and improve the UI on an open source way.

If we could have a priority paving the roads, please help vote for the most critical reason holding you back from hacking a DSO nano:


Please suggest if anything we can do to make this a lot easier. : )

About Author

10 thoughts on "[Survey] What’s holding you back from hacking a DSO nano?"

  1. I found a FAQ in your forum,

    “Is DSO Open source ?
    The F/W of V1.X will be open source and all people can use or modify them freely , but there is some third party code included in V2.X F/W and we don’t have the authorization to publish them.”

    So the way I read this is that the DSO Nano is no longer open source. Is that correct?

    1. 你好

      DSO software is mainly two parts: app & lib. Most of the open source project is based on app, you can make various application upon it.

      The lib is also open by the designer, but it updates when there available update from the designer. You can also contribute to the lib too.

Comments are closed.

Calendar

May 2010
M T W T F S S
 12
3456789
10111213141516
17181920212223
24252627282930
31