Seeed Wiznet Shield issue

Issue: Potential problem for Seeed Wiznet Shield power supply

Root cause: Mistakenly used AMS1117-5 instead of AMS1117-3.3 during production

Coincidence: The design was to use AMS1117-3.3 to provide 3.3V from 5V, but AMS1117-5 is mistakenly used. The 5V input does not meet requirement from AMS1117-5, it coincidently output around 3.4V and made the whole board working fine and passed our validation and test.

Severity: mild. The boards are all tested and proven working, only 2 out of 300 are reported faulty and are not confirmed AMS1117-5 issue. However, there is possibility that the board might fail or working unstable in certain applications.

Follow up: We will extend all wiznet shield warranty to 3 years including free change. If you are feeling uncomfortable  in continue using the board, please send a mail including your order number and address to wiznetissue{at}seeedstudio.com for:

1) Send back the board with mistaken IC for replacement

2) Ask  for  a replacement AMS1117-3.3 if you are OK with the soldering

Thanks douwehomans for pointing this out on our forum http://www.seeedstudio.com/forum/viewtopic.php?f=4&t=688

About Author

Calendar

April 2010
M T W T F S S
 1234
567891011
12131415161718
19202122232425
2627282930