Bus Pirate firmware v3.6 released

Bus Pirate firmware v3.6 is available for download, this is a minor bug fix release. Update using the normal firmware upgrade procedure. This release does not reach into the upper memory page, so there shouldn’t be any upgrade issues. Changes include:

  • Fixed version string. v3.5 displayed ‘Firmware 3.5′ instead of ‘Firmware v3.5′. This caused issues with Bus Pirate support in AVRdude.
  • Added pause with lit MODE and VREG LED to self-test.

Since release v3.1 the Bus Pirate v2go and v3 share the same firmware. Upgrade v2go with the firmware for v3.

Via dangerousprototypes.com

About Author

Calendar

January 2010
M T W T F S S
 123
45678910
11121314151617
18192021222324
25262728293031