Dismantle your DSO nano
Dismantel your DSO nano is pretty easy, but it’s still worth writing a tutorial to let people know what does DSO nano look inside before open it.
Note:
This tutorial is for information purposes, Dismantle the DSO nano and follow this tutorial at your own risk!
You will need:
A sharp knife (Or something else sharply)
A 1.4mm screwdriver
First you need to remove the top panel by using a sharp knife. The top panel is attached with the body by glue, be sure to do this slowly, or you will damage the acrylic panel .
Here you can see 6 screws(marked with white circle) after the top panel is removed. Remove them with a 1.4mm screwdriver, then go to the next step.
Remove the rest 2 screws, now you should be able to take the sub-board apart from the motherboard.
Sub-Board detailed pictures. 6 metal dome buttons were soldered on the top side, and 1×3.5MM TSR connector, 1X Mini usb connector on bottom. There’s also a board to board connector to attach the 2 separated PCB.
Here we go, now you can take the screen and motherboard away from the case.
1. controller: STM32
2. stabilized voltage supply : 3.3V voltage output
3. stabilized voltage supply : 3.0V voltage output
4. stabilized voltage supply : use a P3232 RS-232 transceivers to output +5V and -5V voltage
5. general purpose dual J-FET operation amplifier : to separate and scale the input signal
6. 8-Channel Analog Multiplexer : change the match channel for different V/div