What a GIFT!

I came from a small town which called ‘Rain city’, it rains a lot. After I was in Shenzhen, rain became so rare and I missed it alot. Then when I was taking a nap in this afternoon, Almighty God brought me some ‘gift’, STORM!

I’ve seen lot’s of storm but this one Tops them all! What a ‘gift’! The sky became dark ,the windows was shaking in the wind, i bet there was accident happened in the street.

Eric went to the SEG market right before the storm came, and i’ve no idea how long will it last. Fortunately, the storm only lasted for 1 hour, and he safely came back with some new candies.

This is a nice, really beautiful 128×64 pixel Serial graphical FSTN LCD. The LCD has a light gray background and pixels appear dark gray. Unit comes with an white LED backlight and built-in ST7565(67)  interface controller. LCD and backlight are driven by 3.3V.   Click for more infos

This little joystick is one of my favorite components, it looks pretty much like the Playstation2 analog Joystick. (I am a huge fan of video games) Its Directional movements are simply two potentiometers – one for each axis, and this joystick also has a select button that is actuated when the joystick is pressed down.

Click for more infos

These candies are absolutely sweet!  It comes with 9 LEDs, working with 12V DC.Put it somewhere and light it up, What a beauty!

I was wondering if i can use these to make a necklace for my girlfriend^^ Must be cool if you wear it in party.

Click for more infos

By the way, We produced more UartSB V2.1. It became so popular since it was released. And we changed its color from green to blue, matchs the color of XBee® RF Modules & Blue tooth modules. That’s what i called harmony(和谐).

About Author

Calendar

March 2009
M T W T F S S
 1
2345678
9101112131415
16171819202122
23242526272829
3031