Monome like all-in-oneButton II

This is from a discussion in monome.org. I posted our Monome-like all-in-one button, and evilpaul replied with much bigger ones he had experiened. I recalled about this button, which I have sampled but abandoned for its size. Since there are even more giant ones like using arcade buttons, these ones are pretty OKay then.

Discussion on monome forum:
http://post.monome.org/comments.php?DiscussionID=2346&page=1#Item_21

Evil Paul’s blog:
http://evilpaul.vox.com/library/post/arduinome.html

Product info:
Button Diameter: 13 mm
Shell Diameter: 18 mm
Height(not including pins): 24mm
Pin: 2 for button, 2 for LED
Made in Taiwan

Available >>here

About Author

Calendar

September 2008
M T W T F S S
1234567
891011121314
15161718192021
22232425262728
2930