News monome-like all-in-one button matrix By è¡æ¿ 16 years ago Thanks to Albert’s handwork ð Some photos here: Available here for 1$~~ ^^ About Author è¡æ¿ See author's posts Tags: Arduino, button, monome, Seeeduino Continue Reading Previous FOUNT IT! monome monome monome monome ~~~Next Seeeduino PCB ready~ 9 thoughts on “monome-like all-in-one button matrix” Even there are theses buttons in stock? I can’t find it. Where i can buy some of them? Is there a silicone cover for these buttons? They don’t look so user-friendly by themselves. The buttons are ready now! You can order as many as you want~lol Are you going to get more of these buttons in stock soon? For the PCB we are making for 8*8 matrix, diode is added. Thanks for remindingïŒ: ) … No diodes? no goshting? … It’s a tiny LED come along with the button. We didn’t use Arduinome, the matix is connected to a freeduino. And some simple code to make the demo. No diode yet. ^^ cool. did you use the standard arduinome code or write your own? did you use diodes on the proto board? Those are 3 or 5mm leds ? Comments are closed.
It’s a tiny LED come along with the button. We didn’t use Arduinome, the matix is connected to a freeduino. And some simple code to make the demo. No diode yet. ^^
cool. did you use the standard arduinome code or write your own? did you use diodes on the proto board?
Even there are theses buttons in stock? I can’t find it. Where i can buy some of them?
Is there a silicone cover for these buttons? They don’t look so user-friendly by themselves.
The buttons are ready now! You can order as many as you want~lol
Are you going to get more of these buttons in stock soon?
For the PCB we are making for 8*8 matrix, diode is added.
Thanks for remindingïŒ: )
…
No diodes? no goshting?
…
It’s a tiny LED come along with the button.
We didn’t use Arduinome, the matix is connected to a freeduino. And some simple code to make the demo. No diode yet.
^^
cool. did you use the standard arduinome code or write your own? did you use diodes on the proto board?
Those are 3 or 5mm leds ?