![Loading...](https://static-cdn.seeedstudio.com/static/version1721042825/frontend/bs_complex/bs_complex5/en_US/images/loader-1.gif)
Grove - Multichannel Gas Sensor
Three independent gas channels in one package Built with ATmega168PA Detectable gases include:Carbon monoxide (CO) , Nitrogen dioxide (NO2) , Hydrogen (H2) , Ammonia (NH3) , Methane (CH4) , etc Grove compat
- 10+: $33.00
YOU MAY LIKE THIS
PRODUCT DETAILS
We have updated the product to Multichannel Gas Sensor v2 with more detailed documents and more onboard sensor modules. And we offer a lower price!
Grove – Multichannel Gas sensor is an environment detecting sensor with a built-in MiCS-6814 which can detect many unhealthy gases. 3 gases can be measured simultaneously due to its three channels, so it can help you to monitor the concentration of more than one gas.
This sensor belongs to the Grove system, and you can plug it onto the Base shield and work with Arduino directly without any jumper wires. The interface is I2C, so plug it onto the I2C port of Base shield, then you can start to work on it.
Tip
We've released the Seeed Gas Sensor Selection Guide, it will help you choose the gas sensor that best suits your needs.
Features
-
Three fully independent sensing elements on one package
-
Built with ATmega168PA
-
I2C interface with programmable address
-
Heating power can be shut down for low power
-
Detectable gases: Carbon monoxide (CO), Nitrogen dioxide (NO2), Hydrogen (H2), Ammonia (NH3), Methane (CH4), etc.
One More Thing
With the SenseCAP S2110 controller and S2100 data logger, you can easily turn the Grove into a LoRaWAN® sensor. Seeed not only helps you with prototyping but also offers you the possibility to expand your project with the SenseCAP series of robust industrial sensors.
The IP66 housing, Bluetooth configuration, compatibility with the global LoRaWAN® network, built-in 19 Ah battery, and powerful support from APP make the SenseCAP S210x the best choice for industrial applications. The series includes sensors for soil moisture, air temperature and humidity, light intensity, CO2, EC, and an 8-in-1 weather station. Try the latest SenseCAP S210x for your next successful industrial project.
Technical details
Dimensions | 89mm x140mm x6.8mm |
Weight | G.W 10g |
Battery | Exclude |
Voltage | 3.1~ 5.25V |
Ripple(@Max Power) | 80~100mV |
Max Heating Power | 88mW |
Max Power | 150mW |
ADC Precision | 10Bits |
I2C Rate | 100kHz |
VIL(@I2C) | -0.5~0.99V |
VIH(@I2C) | 2.31~5.2V |
Part List
Grove – Multichannel Gas Sensor | 1 |
26AWG Grove Cable | 1 |
ECCN/HTS
HSCODE | 9027900000 |
USHSCODE | 8517620090 |
UPC | 841454107910 |
COO | CHINA |
RoHS | 1 |
LEARN AND DOCUMENTS
SHARED BY USERS
REVIEWS
-
-
The device unfortunately has an issue where its onboard microcontroller locks up, requiring a hard reset. This means the standard Grove interface can not restore operation. One must solder an additional control wire to the nRST pad on the back of the board and run it to a GPIO on Arduino in order to reset the sensor's microcontroller. Grove devices should work with only I2C.
-
Grove - Multichannel Gas Sensor We love the product works well with Arduino. Sadly, we are struggling to make it work with Raspberry Pi 3 (RPI-3). We believe and think this product would very well with RPI-3 fans.
Furthermore, we use a lot of your Grove Sensors and believe having Grove - Multichannel Gas Sensor work with RPI-3 would a feather in your cap.
With sincere regards & thank you
Dhirendra Damji - AKA Doc Yoda (email - [email protected])
based in Tempe, Phoenix, Arizona, USA
A loyal customer who buy buys directly through your Website -
received in good condition but shipping company charged a lot as extra fee at time of delivery The product is good but the shipping company associated with seeedstudio is not satisfies. Thry charge more that the value of product as custom duty.
The duty charged by government custom was near about the 15 percent of total value they charged. rest they charge as handling fee, other fee and etc.
SEESDSTUDIO should take some action as its not good deal for customer at the end. -
Great Parts Works great.
FAQ
- Page Previous
- Page 1
- You're currently reading page 2