Skip to main content

Xadow - Vibrator Motor

This small vibrator motor can vibrate like your phone. When using it, you only need to power for the module and then send "Vibration" command. In fact, the "Vibration" command is setting control pins to high level, then it will work. I like this module because it can create a short-term shock to prompt me whether one operation was successful, such as shaking my arm to switch my iPhone songs, which sounds terrible, but it does not like the buzzer.

Specification


  • working voltage: 3.3V

  • Rated Speed: 9000rpm

  • controlled by two digital signals

  • Dimensions: 25.43mm x 20.35mm

Demonstration


Here is a Demo Code showing how to turn on the vibration motor.

Hardware Installation:

Note: when connect Xadow Vibrator Motor to Xadow Main Board, you should concern about the connection direction. The connection method is that the unfilled corner of one Xadow module need to connect to the right angle of another module(see four corners of each Xadow module). Demo code like this:

<pre>
void setup()
{
DDRF |= 0x01;
DDRB |= 0x04;
}

void loop()
{
//turn on the vibration motor
PORTF |= 0x01;
PORTB |= 0x04;
delay(1000);
//turn off the vibration motor
PORTF &amp;= ~(0x01);
PORTB |= 0x04;
delay(1000);
//turn on the vibration motor
PORTF |= 0x01;
PORTB |= 0x04;
delay(1000);
//turn off the vibration motor
PORTF |= 0x01;
PORTB &amp;= ~(0x04);
delay(1000);
//turn on the vibration motor
PORTF |= 0x01;
PORTB |= 0x04;
delay(1000);
//turn off the vibration motor
PORTF &amp;= ~(0x01);
PORTB &amp;= ~(0x04);
delay(1000);
}</pre>

Schematic Online Viewer

Resources


Xadow Vibrator Motor Eagle File

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.