Skip to main content

Wifi Bee

Wifi Bee is a xBee Pro socket compatible standalone MCU node useful for Wireless Sensor Network. It integrates Microchip IEEE 802.11 Wi-Fi transceiver module MRF24WB0MA and a 8bit AVR MCU ATMega328P. The smart and xBee Pro Socket compatible outlook makes it very easy to integrate in your product. The ATMega328P could be directly programmed under the open source Arduino IDE when you plug it on to the UartSBee or Grove - XBee Carrier . The SPI pins on MCU are connected to the corresponding pins of MRF24WB0MA to communicate with each other, while some of the other pins (DIO, AD,PWM etc.) are brought out to the 20 pins of 2.0 mm male pin headers. Please note there is no dedicated firmware for Wifi Bee yet now, but you may use the firmware of WiShield from AsyncLabs. Please make sure you can use it before you buy.

Model: WLS48188P

Features

  • xBee compatible headers

  • Programmable using Arduino IDE

  • Arduino Duemilanove bootloader preprogrammed

  • Supports low power and low data rate Wi-Fi.

  • 802.11b compatible

  • WEP, WPA-PSK, WPA2-PSK Security

  • LEDs for PWR and Wi-Fi connection indication.

Application Ideas

  • Wireless Local Area Network

  • Wireless Sensor Network using Grove - XBee Carrier

  • Internet connectivity

  • Build endless network applications with uIP TCP/IP Stack

  • Ideal for people wanting to learn and experiment with TCP/IP Stack

Schematic

Click here to open schematic in PDF format

Key Specification

ItemMinimumTypicalMaximum
Operate voltage3.0V3.3V3.6V
Working temperature0°C to +70°C
Working frequency16MHz
MCUATmega328P

Mechanical Dimensions

Wifi Bee is of 27.2mm x 35.7mm size.

Hardware

Wifi Bee - Parts

Pin definition & Rating

Pin#Pad TypeDescriptionArduino Pin Number
3V31Supply inputVCC, +3.3V-
TX2OutputUart Tx port1(DIO)
RX3InputUart Rx port0(DIO)
PB04Input/OutputATmega328P PB08(DIO)
!RESET5InputATmega328 Reset port
PD76Input/OutputATmega328P PD77(DIO)
PD67Input/OutputATmega328P PD66(DIO)
PD58Input/OutputATmega328P PD55(DIO)
!DTR9InputUsed for programming the ATmega328P-
GND10GNDGND-
PC111Input/OutputATmega328P PC11(Analog input)/15(DIO)
PC012Input/OutputATmega328P PC00(Analog input)/14(DIO)
AD713InputATmega328P ADC77(Analog input)
VREF14InputATmega328P AREF port-
AD615InputATmega328P ADC66(Analog input)
INT116Input/OutputATmega328P PD33(DIO)
PC317Input/OutputATmega328P PC33(Analog input)/17(DIO)
PC218Input/OutputATmega328P PC22(Analog input)/16(DIO)
SCLSCL19Input/OutputATmega328PPC5 5(Analog input)/19(DIO)
SDA20Input/OutputATmega328P PC44(Analog input)/18(DIO)

Usage

Hardware Installation

Grove - XBee Carrier - Connected to Wifi Bee and Powered By USB

Programming

Wireless Network Setup

This section gives a brief overview on setting up a Home Network with a WiFi router suitable for Wifi Bee.

Wireless Sensor Network - Sample Architecture with Wifi Bee Nodes

1.Login to web configuration interface of WiFi router using a web browser. Normally a default IP address like 192.168.0.1 and a Login id:admin and Password:password is provided by the router manufacturer. Use this.

2.In the above case the router IP address 192.168.0.1 is also the Gateway IP Address of the Wireless Network. The subnet mask for this IP address is 255.255.255.0 3.Set a name or SSID for the Wireless Network. Let us set it to HOMENETWORK. This name will be used throughout the tutorial.

4.Any node that connects to a router gets an IP address through DHCP. But, Wifi Bee does not support DHCP. We have to assign a static IP address. Many routers provide address reservation using MAC address for network devices. In LAN setup section of wireless router, reserve IP address 192.168.0.4 for Wifi Bee.

  • 1.Enter the IP address to be reserved as 192.168.0.4. This is the IP address of Wifi Bee
  • 2.You need to enter the MAC address displayed on Wifi Bee in the form of AB:CD:EF:GH:IJ:KL
  • 3.Give the device-name as WIFIBEE. This name can be any word and not very important.

5.Configure the Security options of the Network. Wifi Bee supports Open(Security disabled), WEP (Wired Equivalent Privacy), WPA-PSK (Wi-Fi Protected Access Pre-Shared Key) and WPA2-PSK (Wi-Fi Protected Access 2 with Pre-Shared Key). Set a suitable security option. This setting is used by Wifi Bee for establishing connection.

  • 1.Let us set security option to WPA-PSK.

  • 2.WPA-PSK mode requires WPA-PSK Security Encryption Network Key. Set this key to 12345678

6.Consult the router's user guide for configuring other setting like connecting to internet, etc..

Downloading and configuring the Library for running the application examples

The application examples uses the WiSheild library of Asynclabs. There is no other dedicated firmware for Wifi Bee. This library uses uip TCP/IP stack of Adam Dunkels. This library is provided under GPL v2 by the original author. Hence, any application that could be built with WiShield should also be GPLv2 compatible.

1.Download the library from WiShield.

2.Extract the contents to Arduino /libraries/WiShield directory.

3.The library comes with many application examples. It is written in a configurable manner such that only the required functionality is built. This saves FLASH.

  • This configuration is handled in /libraries/WiShield/apps-conf.h.

  • Uncomment the desired mode for the application that you are building like WEB-SERVER or WEB-CLIENT or SOCKET Application, etc.. in /libraries/WiShield/apps-conf.h file.

  • For example if you want to build a Web Server Application the #define APP_WEBSERVER should have been uncommented and all other modes are commented. These change requires rebuild of the library. Hence close and re-open Arduino IDE.

4.Let us build the WebServer example.

  • Set the mode configuration as APP_WEBSERVER in /libraries/WiShield/apps-conf.h.

  • Open /libraries/WiShield/examples/WebServer/WebServer.pde sketch in Arduino IDE

  • Set the local_ip[] array to {192,168,0.4}. This the IP address Wifi Bee as configured above.

  • Set the gateway_ip[] array to {192,168,0,1}. This is the router's IP address as configured in network setup above.

  • Set the subnet_mask[] array to {255,255,255,0}. This is the sub-net mask for the local wireless network.

  • Set prog_char ssid[] to {"HOMENETWORK"}. This name was also assigned during network setup.

  • Next step is to set the security_type to security options configured during network setup. Set to 2 (i.e WPA) as configured in Wifi router.

  • //unsigned char security_type = 2; // 0 - open; 1 - WEP; 2 - WPA; 3 - WPA2

  • Also set const prog_char security_passphrase[] PROGMEM = {"12345678"}

5.The modified WebServer.pde sketch looks like the code listed below.

6.Set the board type to Arduino Duemilanove and compile the sketch.

7.Upload it Wifi Bee and press the Reset button

8.If every thing goes fine the Wifi Bee connects to HOMENETWORK and the BLUE LED (WIFI LED) glows

9.Open a web browser from a PC connected to HOMENETWORK and type the URL [http://192.168.0.4]

10.You would get the message Hello World!! I am WifiBee.

/*
* Web Server: Modified WebServer.pde example.
* A simple web server example using the WiShield library and WiBee.
*/

#include <WiShield.h>

#define WIRELESS_MODE_INFRA 1
#define WIRELESS_MODE_ADHOC 2

// Wireless configuration parameters ----------------------------------------
unsigned char local_ip[] = {192,168,0,4}; // IP address of Wifi Bee
unsigned char gateway_ip[] = {192,168,0,1}; // router or gateway IP address
unsigned char subnet_mask[] = {255,255,255,0}; // subnet mask for the local Wireless network
const prog_char ssid[] PROGMEM = {"HOMENETWORK"}; // max 32 bytes

unsigned char security_type = 2; // 0 - open; 1 - WEP; 2 - WPA; 3 - WPA2

// WPA/WPA2 passphrase
const prog_char security_passphrase[] PROGMEM = {"12345678"}; // max 64 characters. The network name.

// WEP 128-bit keys
// sample HEX keys
prog_uchar wep_keys[] PROGMEM = { 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08, 0x09, 0x0a, 0x0b, 0x0c, 0x0d, // Key 0
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, // Key 1
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, // Key 2
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 // Key 3
};

// setup the wireless mode
// infrastructure - connect to AP
// adhoc - connect to another WiFi device
unsigned char wireless_mode = WIRELESS_MODE_INFRA;

unsigned char ssid_len;
unsigned char security_passphrase_len;
//---------------------------------------------------------------------------

void setup()
{
WiFi.init();
}

// This is the webpage that is served up by the webserver
const prog_char webpage[] PROGMEM = {"HTTP/1.1 200 OK\r\nContent-Type: text/html\r\n\r\n<center><h1>Hello World!! I am WifiBee.</h1></center>"};

void loop()
{
WiFi.run();
}

Examples

Simple Web Server that sends sensor value to Web browser

  • Use the network setup as describe above.

  • Use the Grove - XBee Carrier for programming and power.

  • Configure apps-conf.h, such that only APP_WISERVER mode is used.

  • Compile and upload the following sketch to Wifi Bee using Arduino IDE as described for above example.

  • Press the reset button. Wait for the Wifi Bee to connect to WiFi network (Blue LED glows).

  • Verbose information of the network communication can be seen; if, serial port terminal is open in Arduino IDE (with 57600 baud).

  • Open a web browser from a PC connected to HOMENETWORK and type the URL [http://192.168.0.4]

  • WifiBee serves the Sensor value to browser. The HTML code is written in such a way that it auto refreshes every 10 seconds.

/*
* A simple sketch that uses WiServer and Seeedstudios Wifi Bee to serve a webpage.
* An analog sensor is connected to A2 of Wifi Bee (use Grove - XBee Carrier). This value is sent to the
* client (a web browser). The HTML page is prepared based on sensor value. It also has direction
* to refresh itself automatically.
*/

/*This example is based on SimpleServer.pde. Copyrights rests with original author */

/* for this example to work, modify apps-conf.h file as below ; only APP_WISERVER mode is enabled :
--------------------------------------------------------------------

//Here we include the header file for the application(s) we use in our project.
//#define APP_WEBSERVER
//#define APP_WEBCLIENT
//#define APP_SOCKAPP
//#define APP_UDPAPP
#define APP_WISERVER
----------------------------------------------------------------------
*/

#include <WiServer.h>

#define WIRELESS_MODE_INFRA 1
#define WIRELESS_MODE_ADHOC 2

// Wireless configuration parameters ----------------------------------------
unsigned char local_ip[] = {192,168,0,4}; // IP address of WifiBee
unsigned char gateway_ip[] = {192,168,0,1}; // router or gateway IP address
unsigned char subnet_mask[] = {255,255,255,0}; // subnet mask for the local network
const prog_char ssid[] PROGMEM = {"HOMENETWORK"}; // max 32 bytes

unsigned char security_type = 2; // 0 - open; 1 - WEP; 2 - WPA; 3 - WPA2

// WPA/WPA2 passphrase
const prog_char security_passphrase[] PROGMEM = {"12345678"}; // max 64 characters

// WEP 128-bit keys
// sample HEX keys
prog_uchar wep_keys[] PROGMEM = { 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08, 0x09, 0x0a, 0x0b, 0x0c, 0x0d, // Key 0
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, // Key 1
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, // Key 2
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 // Key 3
};

// setup the wireless mode
// infrastructure - connect to AP
// adhoc - connect to another WiFi device
unsigned char wireless_mode = WIRELESS_MODE_INFRA;
unsigned int sensorValue;
unsigned char ssid_len;
unsigned char security_passphrase_len;
// End of wireless configuration parameters ----------------------------------------

int counter;
// This is our page serving function that generates web pages
boolean sendMyPage(char* URL) {

// Check if the requested URL matches "/"
if (strcmp(URL, "/") == 0) {
// Use WiServer's print and println functions to write out the page content
WiServer.print("<html>");

// Instruct the web broweser to refersh every 10 seconds
WiServer.print("<head><meta http-equiv=\"refresh\" content=\"10\"> </head>");
WiServer.println("<H1>WifiBee Connected...<H1>");
WiServer.print("<H2>Sensor Value = ");
WiServer.print(sensorValue); //A2 is connected to an exernal sensor. The RAW value is send to the client.
WiServer.print("</H2></html>");
return true;
}
// URL not found
return false;
}

void setup() {

// Initialize WiServer and have it use the sendMyPage function to serve pages
WiServer.init(sendMyPage);

// Enable Serial output and ask WiServer to generate log messages (optional)
Serial.begin(57600);
WiServer.enableVerboseMode(true);
}

void loop(){
sensorValue = analogRead(A2); //A2 is connected to an exernal sensor via Grove interface in Grove - XBee Carrier .
// Run WiServer
WiServer.server_task();
delay(10);
}

Simple Web Client that sends sensor feeds to Pachube.com

This section will be revised later

  • Use the network setup as describe above.

  • Use the Grove - XBee Carrier for programming and power.

  • Configure apps-conf.h, such that only APP_WISERVER mode is used.

  • Compile and upload the following sketch to Wifi Bee using Arduino IDE as described for above example.

  • Press the reset button. Wait for the Wifi Bee to connect to WiFi network (Blue LED glows).

  • Verbose information of the network communication can be seen; if, serial port terminal is open in Arduino IDE (with 57600 baud).

  • Wifi Bee periodically feeds the data to Pachube.com

/*
* A simple sketch that uses WiServer library and Seeedstudio's WifiBee to send sensor
* feed to pachube.com ;
* This is modified version SimpleClient.pde. Copyright rests with original author.
*/

/* for this example to work, modify apps-conf.h file as below ; only APP_WISERVER mode is enabled :
--------------------------------------------------------------------
//Here we include the header file for the application(s) we use in our project.
//#define APP_WEBSERVER
//#define APP_WEBCLIENT
//#define APP_SOCKAPP
//#define APP_UDPAPP
#define APP_WISERVER
----------------------------------------------------------------------
*/


#include <WiServer.h>

#define WIRELESS_MODE_INFRA 1
#define WIRELESS_MODE_ADHOC 2

// Wireless configuration parameters ----------------------------------------
unsigned char local_ip[] = {192,168,0,4}; // IP address of WifiBee
unsigned char gateway_ip[] = {192,168,0,1}; // router or gateway IP address
unsigned char subnet_mask[] = {255,255,255,0}; // subnet mask for the local network
const prog_char ssid[] PROGMEM = {"HOMENETWORK"};// max 32 bytes

unsigned char security_type = 2; // 0 - open; 1 - WEP; 2 - WPA; 3 - WPA2

// WPA/WPA2 passphrase
const prog_char security_passphrase[] PROGMEM = {"12345678"}; // max 64 characters

// WEP 128-bit keys
// sample HEX keys
prog_uchar wep_keys[] PROGMEM =
{ 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08, 0x09, 0x0a, 0x0b, 0x0c, 0x0d, // Key 0
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, // Key 1
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, // Key 2
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 // Key 3
};

// setup the wireless mode
// infrastructure - connect to AP
// adhoc - connect to another WiFi device
unsigned char wireless_mode = WIRELESS_MODE_INFRA;

unsigned char ssid_len;
unsigned char security_passphrase_len;
// End of wireless configuration parameters ----------------------------------------


// Function that prints data from the server
void printData(char* data, int len) {

// Print the data returned by the server
// Note that the data is not null-terminated, may be broken up into smaller packets, and
// includes the HTTP header.
while (len-- > 0) {
Serial.print(*(data++));
}
}

int sensorValue=0;
//Prepare data to the feed
void pachubefeedData()
{
sensorValue=analogRead(A2); //Read analog sensor connected to A2 (Use Grove - XBee Carrier interface)
WiServer.print(sensorValue);
}



// IP Address for pachube.com
uint8 ip[] = {173,203,98,29};

char hostName[] = "www.pachube.com\nX-PachubeApiKey: YOUR_API_KEY_HERE\nConnection: close"; // Replace YOUR_API_KEY_HERE , with your API key
char url[] = "/api/12345.csv?_method=put"; //Replace 12345 with your feed number

// A request that POSTS data to Pachube
POSTrequest postPachubeFeed(ip, 80, hostName, url, pachubefeedData);


void setup() {
// Initialize WiServer (we'll pass NULL for the page serving function since we don't need to serve web pages)
WiServer.init(NULL);

// Enable Serial output and ask WiServer to generate log messages (optional)
Serial.begin(57600);
WiServer.enableVerboseMode(true);

// Have the processData function called when data is returned by the server
postPachubeFeed.setReturnFunc(printData);
}


// Time (in millis) when the data should be retrieved
long updateTime = 0;

void loop(){

// Check if it's time to send an update
if (millis() >= updateTime) {
postPachubeFeed.submit();
// Send another update after a min
updateTime += 60;
}

// Run WiServer
WiServer.server_task();

delay(10);
}

Bill of Materials (BOM) /parts list

PartQuantityValuePackage
C1110uC_TAN_3X3.5
C2,C321u0603
C41100n0603
J11CK_2X3_2.0CK_2X3_2.0
PWR1redLED0603
R1110k0603
R2,R3,R4,R5,R754.7k0603
R611k0603
U11OPEN_BEEXBEE_EXT_SMD
U31MRF24WB0MAMRF24WB0MA
U41ATmega328P_MU1040MLF32X
WIFI1blueLED0603
X1116MHzXTAL_3X2

Support

If you have questions or other better design ideas, you can go to our forum or wish to discuss.

Version Tracker

RevisionDescriptionsRelease
v0.91bInitial public releaseApril 6, 2011
v1.0Change the width of the signal wire from 6 mil to 8 milDec 13, 2011

WifiBee v1.0 Schematic Online Viewer

WifiBee v0.91b Schematic Online Viewer

Resources

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.