Grove - Moisture Sensor

From Wiki
Jump to: navigation, search

Contents

Introduction

This Moisture Sensor can be used to detect the moisture of soil or judge if there is water around the sensor, let the plants in your garden reach out for human help. They can be very easy to use, just insert it into the soil and then read it. with help of this sensor, it will be realizable to make the plant remind you : hey, i am thirsty now, please give me some water.

Model: SEN92355P

Moisture sensor .jpg

Features

  • Soil moisture sensor based on soil resistivity measurement
  • Easy to Use
  • 2.0cmX6.0cm grove module

Specification

Item Condition Min Typical Max Unit
Voltage - 3.3 / 5 V
Current - 0 / 35 mA
Output Value Sensor in dry soil 0 ~ 300 /
Sensor in humid soil 300 ~ 700 /
Sensor in water 700 ~ 950 /

Application Ideas

  • Botanical gardening
  • Moisture sensoring

Usage

This is a summary of the moisture sensor can be used to detect the moisture of the soil, when the soil moisture deficit, the sensor output value will decrease. You can know whether a plant needs water by observing the results that the sensor output. The following sketch demonstrates a simple application of sensing the moisture of the soil.

  • Connect this module to one of analog port A0 of Grove - Base Shield with the 4 pin Grove cable, and then insert the Sensor into the soil or place it anywhere you want.
  • Plug Grove - Base Shield into the Arduino/Seeeduino and connnect Arduino to PC via a USB cable.

The hardware installation as show below:
Moisture1.jpg
Note:This sensor isn't hardened against contamination or exposure of the control circuitry to water and may be prone to electrolytic corrosion across the probes, so it isn't well suited to being left in place or used outdoors.

  • Copy and paste code below to a new Arduino sketch.
int sensorPin = A0;    // select the input pin for the potentiometer
int sensorValue = 0;  // variable to store the value coming from the sensor

void setup() {
  // declare the ledPin as an OUTPUT:
   Serial.begin(9600);  
}

void loop() {
  // read the value from the sensor:
  sensorValue = analogRead(sensorPin);    
  delay(1000);          
  Serial.print("sensor = " );                       
  Serial.println(sensorValue);                   
}
  • Upload the code, Please click here if you do not know how to upload.
  • The Result in different condition after open the serial monitor:
No load.jpg Dry soil.jpg Humility soil.jpg IN water.jpg
Sensor in air Sensor in dry soil Sensor in humid soil Sensor in water

Version Tracker

Revision Descriptions Release
v0.9b Initial public release 13,Sep,2011

Resources

Support

If you have questions or other better design ideas, you can go to our forum or wish to discuss.

Personal tools
Namespaces

Variants
Actions
Structure
Seeed Products
Support
Toolbox