Please do not refresh the page while your request is being processed.
Stencil Cost
USD$0.00
Sub-Total
USD$0.00
Production Time
Working Days
Weight
Shipping Calculated at Checkout
Tips
Production time is the time period between file confirmation phase to ready for packing(Note:File reviewing is not included).Learn More
Please make sure the effective area should be larger than PCB size.
Sides of the PCB to be etched on the stencil. When choosing option 3, please ensure that the effective area is large enough to fit both sides. For the fourth option, the quantity of stencils must be an even number.
The quantity of stencil.
Fiducial Mark is designed to help the machine to check the location.
Stencil thickness will determine the amount of solder paste left on your PCB .
BGA plating is also called Electropolishing. If your board has BGA, we highly recommend you to choose BGA Plating.
Production time is the time period between file confirmation phase to ready for packing(Note:File reviewing is not included).Learn More