[size=150]Using GPRS Shield With Mega[/size]
- Connect pin-7 to pin-10 (pin-8 to pin-11) by jumper wire
- Use this code:
#include <SoftwareSerial.h>
SoftwareSerial GPRS(10, 11);
unsigned char buffer[64]; // buffer array for data recieve over serial port
int count = 0; // counter for buffer array
void setup()
{
GPRS.begin(19200); // the GPRS baud rate
Serial.begin(19200); // the Serial port of Arduino baud rate.
}
void loop()
{
if (GPRS.available()) // if date is comming from softwareserial port ==> data is comming from gprs shield
{
while (GPRS.available()) // reading data into char array
{
buffer[count++] = GPRS.read(); // writing data into array
if (count == 64)
break;
}
Serial.write(buffer, count); // if no data transmission ends, write buffer to hardware serial port
clearBufferArray(); // call clearBufferArray function to clear the storaged data from the array
count = 0; // set counter of while loop to zero
}
if (Serial.available()) // if data is available on hardwareserial port ==> data is comming from PC or notebook
GPRS.write(Serial.read()); // write it to the GPRS shield
}
void clearBufferArray() // function to clear buffer array
{
for (int i=0; i < count; i++)
{
buffer[i] = NULL;
} // clear all index of array with command NULL
}
- Go AT command tester describe in product wiki, Connect with 19200 bps
Note:Don’t forget to plug the jumpers to SWserial mode.
Good luck!